Reply

Installation error 1935


I'm trying to install SE2DDraft.exe on a notebook that is running Vista. I currently
have it installed on an XP operation system with no problems. On the Vista machine
I get an install error 1935, 'Microsoft.VC80.ATL,type="win32",version="8.0.50727.762",publicKeyToken="1fc8b3b9a1e18e3b",processorArchitecture="x86"".
I did a search on MS web help and forum and got nothing that meant anything to
me. Any help?
1 REPLY

Re: Installation error 1935

Quinten,
Isn't Vista a blast??? Not!!!
Installing 2D Drafting will also install some needed Microsoft resources
(Dot Net Framework). These are needed components for the software to run
properly. The error is a Microsoft installation error when .NET fails to
install.
I did some research and there can be a number of causes. One thing I found
as a possible solution is to install .NET directly and then install Solid
Edge 2D Drafting. Go to the following web site and follow the directions to
see if you can install the .NET Framework Version 2.0 directly. Follow the
instructions on the web page. Let me know if you get the same error
installing it directly.
http://www.microsoft.com/downloads/details.aspx?familyid=0856eacb-4362-4b0d-8edd-aab15c5e04f5&displa...
Once .NET is installed, the installation of Solid Edge 2D Drafting will skip
that step. Try installing 2D Drafting again.
Let me know how it works.
Regards,
Rick B.