Installing ST3 : missing file ?

N/A
Hello all,

The " SE2DDraftV103FRENCH.exe " has been downloaded and launched. By clicking on the "Setup.exe" file, The OS warns that the "...\SE2DDRaftingV103\install\System~1.cab" cannot be found. If i choose to "cancel", the installing procedure stops. If i choose to "retry", the installing procedure does not go on anymore.

My environnement is : XP SP3 , Net Framework 3.5 SP1

Thanks for any help.

Pierre.
1 REPLY

Re: Installing ST3 : missing file ?

N/A
Pierre,
I am investigating this.
At this point this is something I have not seen.
Are you installing the software locally to the machine, not across a
network?
The executable unzips itself when you run it.
It will put down temporary installation files.
It will prompt where to put these files.
Take the default.
The file specified is one of these temporary files.
Regards,
Rick B.