Cancel
Showing results for 
Search instead for 
Did you mean: 

Intellisketch ST9 2d not working in one of the user profiles under Windows7

Creator
Creator

Hi,

 

I have a problem with Intelli Sketch where it is not working, (when you hoover over a line the expected icons to indicate line or mid point do not appear) the appropriate boxes in intellisketch are selected) I have un installed and registry cleaner, deleting directory under c:\program files\solid Edge ST9 and re installed, 

I have found that it is related to only one user prifile, I would assume there is a corruption in this profile for the files related to ST9 and need to delete these, can some one help me with this.

 

Regards Mike

2 REPLIES

Re: Intellisketch ST9 2d not working in one of the user profiles under Windows7

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi @mikewnz,

pls explain what you mean with "user profile". 

Maybe this is the wrong forum (2D Drafting)

 

Edit: sorry, I did mix up 3D profiles with windows profiles Smiley Wink

 

To solve the problem with one windows user profile  you could delete the Registry Key 

Computer\HKEY_CURRENT_USER\Software\Unigraphics Solutions\Solid Edge\Version 109

 

!! Be shure to be in the Current_User HIVE and save a backup before you delete.

Close Solid Edge before you do it!

When you start Solid Edge after that you have all the default settings.

regards

JB
VS2015, SE ST10

Betreff: Intellisketch ST9 2d not working in one of the user profiles under Windows7

Honored Contributor
Honored Contributor

Hi @mikewnz

 

 

just take a view into the Intelligent Options of that user. wether o rnot the mouse options are turned of to show element points

 

20171020_2100.PNG



regards
Wolfgang