Reply

Is there an easy way to subdivide a line?

I have an operation that i use very often. I need to take a line or a distance between 2 points and equally sub-divide it to find a pacing that works.

 

what i do now is insert points and them space then manually by dividing the line length, but it is vert time consuming.

is there a feature like autocad that can divide a line into a number of equally spaced points or segments?

 

thanks for your help

1 REPLY

Re: Is there an easy way to subdivide a line?

not a single command.

 

but you can use retangular pattern with option "fit to rectangle"... this at least auto calculate your equally divided segments

 

 then use the split command...

 

 

 

===================================================
Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
NX10 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.6