Layer Properties

N/A

Layers: when you right click the layer in the edge bar and select properties, there's
an option to add properties/attributes, but the help function doesn't give any indication
of what types of things you can add in here/what they'll do. Can anyone else enlighten
me!?
Cheers guys
Simon
2 REPLIES

Re: Layer Properties

N/A

Simon,
Most all objects have property tags. These are just user defined attributes to use
as you wish. If you draw a line and go to Properties of the line and then click
on the User Tab in the properties dialog, you will see the same UI to add user defined
properties to the line. In full Solid Edge you could write a VB program to apply
or look for these user defined attributes.
Regards,
Rick B.

Re: Layer Properties

N/A

So is there any way we can define a property or variable to turn the layers off or
on?
I can't see Boolean as a variable type.
Cheers,
-AS
www.continual-motion.com