Highlighted

Malware included?

N/A

I try to keep my PC as free from spyware/malware as possible and I find that the
malware "Backdoor.bot" is in my version of SolidEdge.
When I remove it I keep getting error messages.When I restore it I no longer get
the error messages.
Is this something that Solid Edge include in the software from the outset?
Regards,Allan Waterfall.
2 REPLIES

Re: Malware included?

N/A
Allan,
I can assure you that Solid Edge does NOT include any virus or malware upon
installation. Are the errors when you run Solid Edge or other applications?
Regards,
Rick B.

Re: Malware included?

N/A

"Ricky Black" wrote:
>Allan,
>I can assure you that Solid Edge does NOT include any virus or malware upon
>
>installation. Are the errors when you run Solid Edge or other applications?
>
>Regards,
>Rick B.
>
>

Hi Rick,
Thanks for the reply.I ran my anti malware program and it came up with that Backdoor.Bot
and Solid Edge threw up repeated warnings when I removed it.
Anyway I've now gone back to V.20 because I find the interface more user friendly,I
struggled to find the tools I wanted to use in the latest version unfortunately,and
V.20 just seems more user friendly to me.
I'm only an occasional user and having all the tools on the left hand side and top
suits my way of working,I seemed to be going all over the screen with the latest
version.
Regards,Allan Waterfall