Many, many holes

N/A
I have been using SE Free2D for a couple of months now and I must it is a very good program. I have recently come upon a problem that I cannot resolve. It is my lack of knowledge and not the software that is the issue. I need to draw multiple holes centered on increasingly larger diameter circles. All the holes are the same size but on the first circle there will be 9 holes, on the next larger circle there will be 11 holes, on the next circle there will be 17 holes and so on. Is there an easy way to do this? I have searched the forum for the answer and maybe it's there but I don't realize it.
Any help would be appreciated.
Thanks,
Dave
4 REPLIES

Re: Many, many holes

N/A

Dave,
If I understand what you are trying to do, I would use the circular pattern tool.
See attached image. It was done using that tool. Is that what you are trying to
accomplish?
Ed
dcollins@memc.com wrote:
>
>I have been using SE Free2D for a couple of months now and I must it is
>a very good program. I have recently come upon a problem that I cannot
>resolve. It is my lack of knowledge and not the software that is the
>issue. I need to draw multiple holes centered on increasingly larger
>diameter circles. All the holes are the same size but on the first
>circle there will be 9 holes, on the next larger circle there will be 11
>holes, on the next circle there will be 17 holes and so on. Is there an
>easy way to do this? I have searched the forum for the answer and maybe
>it's there but I don't realize it.
>Any help would be appreciated.
>Thanks,
>Dave
>
>
>--
>dcollins@memc.com
>------------------------------------------------------------------------
>dcollins@memc.com's Profile: http://bbsnotes.ugs.com/vbulletin/member.php?userid=38710
>View this thread: http://bbsnotes.ugs.com/vbulletin/showthread.php?t=41283
>


Re: Many, many holes

N/A
Yes, that is exactly what I am trying to do. Can I specify the number of holes per circle and have them evenly spaced? I can't find the circular pattern tool.
Thanks,
Dave

Re: Many, many holes

N/A
I found the circular pattern tool. It work's great. Thank you very much for your help.
Thanks again,
Dave

Re: Many, many holes

N/A
Dave,
It's on the drop list of commands beside the Mirror command.
You preselect the object(s) you want to pattern before you run the command.
Regards,
Rick B.