Reply

Markup and Viewer

I just took a look at the Solid Edge viewer that come with the free version. All of the icons related to the markup function will not work. Is this the way it should be for the free version? Or is there something that I need to setup so the markup features will work?
Rich
2 REPLIES

Re: Markup and Viewer

Rich,
This is correct. The free viewer has the markup capability disabled.
Solid Edge users have what is called View and Markup that enables the markup
capability.
Regards,
Rick B.

Re: Markup and Viewer

I found out some more information.
If you get a .PCF file from someone (Solid Edge User) that is enabled for
markup,
you will be able to open the .PCF file and do measurments.
However, you will not be able to save the file.
If you open directly a native Solid Edge file (.PAR, .ASM, .etc)
all the markup capability is disabled.
Regards,
Rick B.