Reply

Mozilla Thunderbird

Hi,
I currently use Outlook Express as my news reader and it works fine with
private.se_free2d. I want to move to Mozilla Thunderbird but I have been
unable to set it up. Does any body else use Thunderbird? If so, I would be
very grateful to receive some guidance on how to set it up.
My problem may be because the news reader needs to be NNTP compliant. I do
not know what that is and therefore I do not know if Thubnderbird satisfies
that requirement.
Thanks for any help there may be.
Regards
Don.

2 REPLIES

Re: Mozilla Thunderbird

Don Rutherford wrote:
> Hi,
> I currently use Outlook Express as my news reader and it works fine with
> private.se_free2d. I want to move to Mozilla Thunderbird but I have been
> unable to set it up. Does any body else use Thunderbird? If so, I would be
> very grateful to receive some guidance on how to set it up.
> My problem may be because the news reader needs to be NNTP compliant. I do
> not know what that is and therefore I do not know if Thubnderbird satisfies
> that requirement.
> Thanks for any help there may be.
> Regards
> Don.
>
>
>

Hi Don,
I too use Mozilla Thunderbird as my email client plus I use it as my
newsreader for the SE2D forum.
You can go into Tools - Account Settings - and add an account for this
service. Give it a name like 'Solid Edge'.
Some specific settings:
For Outgoing Server (SMTP) I used the default setting which is also my
normal email SMTP server.
For Server Settings: the Server Type is News Server NNTP; the Server
Name is 'bbsnotes.ugs.com'.
Most of the other settings are not critical for this. Once you have
these set-up you should see another inbox called 'Solid Edge' at the
bottom of your Local Folders containing the 'p.se_free2d' forum.
Let me know if you need more info.
Cheers, Rick

Re: Mozilla Thunderbird

On 03/01/2010 12:46, Rick Clise wrote:
> Don Rutherford wrote:
>> Hi,
>> I currently use Outlook Express as my news reader and it works fine
>> with private.se_free2d. I want to move to Mozilla Thunderbird but I
>> have been unable to set it up. Does any body else use Thunderbird? If
>> so, I would be very grateful to receive some guidance on how to set it
>> up.
>> My problem may be because the news reader needs to be NNTP compliant.
>> I do not know what that is and therefore I do not know if Thubnderbird
>> satisfies that requirement.
>> Thanks for any help there may be.
>> Regards
>> Don.
>>
>>

> Hi Don,
>
> I too use Mozilla Thunderbird as my email client plus I use it as my
> newsreader for the SE2D forum.
>
> You can go into Tools - Account Settings - and add an account for this
> service. Give it a name like 'Solid Edge'.
>
> Some specific settings:
>
> For Outgoing Server (SMTP) I used the default setting which is also my
> normal email SMTP server.
>
> For Server Settings: the Server Type is News Server NNTP; the Server
> Name is 'bbsnotes.ugs.com'.
>
> Most of the other settings are not critical for this. Once you have
> these set-up you should see another inbox called 'Solid Edge' at the
> bottom of your Local Folders containing the 'p.se_free2d' forum.
>
> Let me know if you need more info.
>
> Cheers, Rick
>
Hi Rick,
Many thanks for your help. This reply has been done via Thunderbird. So
all systems are go.
Regards, Don.