Reply

New Template windows 7

When I go to the "new" command under the application button and then select the "more" tab I have no templates. When I searched these forums I could find how to do this in vista but it seems different than 7
1 REPLY

Re: New Template windows 7

Are you running with the UAC (User Account Control) enabled or disabled?
It is best to install and run with this disabled. Most likely the UAC is
prohibiting these from being seen in the program folder.
Regards,
Rick B.