PRINTING 1:1 SCALE

N/A

I thought I knew how to print 1:1 scale until now. I'm trying to do so from the
Model page. When I try either the Print Area or As Displayed and correct the default
scale numbers so they show as 1:1, I get output that is slightly different depending
on how much of the image I've selected to print.
Can this be done be done reliably to produce an exact 1:1 output to the printer
or do I have to use the Draft environment?
PS: I'm now using the 102 version and like the improvements. However, I've noticed
a minor bug. When setting up speed keys, some commands are shown more than once
in the pick field. It doesn't seem to matter which I chose but it may confuse the
less literate of us.
Thanks,
Ron
Ronald W Latour
2 REPLIES

Re: PRINTING 1:1 SCALE

N/A
Ron,
You cannot print 1:1 scale directly from 2D Model.
However, you can place a 2D Model View on a working sheet at 1:1 scale and
print from there.
Regards,
Rick B.

Re: PRINTING 1:1 SCALE

N/A

"Ricky Black" wrote:
>Ron,
>You cannot print 1:1 scale directly from 2D Model.
>However, you can place a 2D Model View on a working sheet at 1:1 scale and
>
>print from there.
>
>Regards,
>Rick B.
>

Ricky, thanks. I had a feeling that was the case but I couldn't find the answer
in HELP.
Ron
Ronald W Latour