PURPOSE OF POINT COMMAND

N/A

What is the purpose of the Point Command? When I set a point that is not on a line,
I can't even find it unless I select around the area I placed it. It shows up well
only when I place it on a line. Is it meant to be a drawing element or a construction
reference? I read that is the latter but how do I use it if I can't find it?
Thanks,
Ron
Ronald W Latour
2 REPLIES

Re: PURPOSE OF POINT COMMAND

N/A
Increase point Font so you can see and select them better.

"Ronald W Latour" wrote in message news:48b5ca19$1@bbsnotes.ugs.com...
>
> What is the purpose of the Point Command? When I set a point that is not on a line,
> I can't even find it unless I select around the area I placed it. It shows up well
> only when I place it on a line. Is it meant to be a drawing element or a construction
> reference? I read that is the latter but how do I use it if I can't find it?
>
> Thanks,
> Ron
> Ronald W Latour

Re: PURPOSE OF POINT COMMAND

N/A

David, Got it. Did it. But didn't "think" that the point was a line size. Makes
sense since its grouped with the line command. However, there seems to be an upper
limit. I tried exagerated sizes and found that anything over 3 to 5 mm has no affect
on the point appearance.
I guess the points are just another element.
Thanks,
Ron
"David Rieschick" wrote:
>
>
>
>------=_NextPart_001_0022_01C908E6.5F4FB7D0
>
>Increase point Font so you can see and select them better.
>
>
>"Ronald W Latour" wrote in message =
>news:48b5ca19$1@bbsnotes.ugs.com...
>>=20
>> What is the purpose of the Point Command? When I set a point that is =

>not on a line,
>> I can't even find it unless I select around the area I placed it. It =

>shows up well
>> only when I place it on a line. Is it meant to be a drawing element or =

>a construction
>> reference? I read that is the latter but how do I use it if I can't =

>find it?
>>=20
>> Thanks,
>> Ron =20
>> Ronald W Latour

>------=_NextPart_001_0022_01C908E6.5F4FB7D0
>
>
>
><meta http-equiv="3DContent-Type" content="3D"text/html;" />>charset=3Diso-8859-1">
><meta content="3D"MSHTML" 6.00.2900.3395="" />
>
>
>
>
Increase point Font so you can see and =
>select them=20
>better.

>
 

>
3D"">src=3D"cid:001c01c90910$482104e0$68fa140a@macequipment.com" =
>align=3Dbaseline=20
>border=3D0>

>>
> What =
>is the purpose=20
>of the Point Command?  When I set a point that is not on a =
>line,
> I=20
>can't even find it unless I select around the area I placed it.  It =
>shows=20
>up well
> only when I place it on a line. Is it meant to be a =
>drawing=20
>element or a construction
> reference?  I read that is the =
>latter but=20
>how do I use it if I can't find it?
>
> Thanks,
> =
>Ron =20
>
> Ronald W Latour

>
>------=_NextPart_001_0022_01C908E6.5F4FB7D0--
>
Ronald W Latour