Reply

Print Tiling


Can someont tell me if SolidEdge 2D supports print tiling. I want to print a drawing
24x36 using 8.5 x 11 paper.
Also, when I use the drawing area setup dialog and click OK, it doesnt get saved.
Next time I click this dialog, it reverts to default settings.
3 REPLIES

Re: Print Tiling

Bob,
You should have no problem printing your 24x36 drawing to 8.5 x 11. What
specifically is the problemyou are seeing?
Regards,
Rick B.

Re: Print Tiling


Hi Rick,
Thanks for the reply. I want to print my drawing as 24x36 using an 8.5x11 printer.
I think the usual term for this is print tiling, where a series of 8.5x11 sheets
are generated which are then pasted together to make 24x36.
Can we do this with SolidEdge 2d?
Cheers,
Bob

"Rick B." wrote:
>Bob,
>You should have no problem printing your 24x36 drawing to 8.5 x 11. What
>specifically is the problemyou are seeing?
>
>Regards,
>Rick B.
>
>

Re: Print Tiling

Bob,
Thanks for the description.
Currently there is not an option for this type of printing.
Regards,
Rick B.