Reply

Print to Scale?

Is there a way to print a simple 2d model to scale as in 1:1? This would be on a standard printer, 8.5 x 11 or 11 x 17, no drawing border.
2 REPLIES

Re: Print to Scale?

This should not be a problem as long as you are printing from the Working Sheet (as in Sheet 1). You need to make sure that Sheet 1 is set up as a 8.5 x 11 sheet, though. Do so by going to the Applicaiton Button (top left corner of SE window) and selecting Sheet Setup. On the Size tab, select the Standard radio button then choose A Wide. Click OK, then go back to the Sheet Setup dialog, go to the Background tab and select the blank line from the "Background Sheet" dropdown list. Anything that is drawn on this sheet will print exactly as it is drawn.

Hope this helps.

Andy

Re: Print to Scale?

That works! Thanks!