Printing

N/A

There is no print option on the application menu. How do I print?
Can't find rotate function as described in help?
How can I change default settings so units will default to inches?
1 REPLY

Re: Printing

N/A
1. See attached Print.png image and confirm that your option is missing
2. See attached Rotate.png image. The Rotate command is located on the
sketch tab
3. Start with the ANSI Draft template. If you installed with ISO as your
default templates then you will find the ANSI Draft template on the More tab
after clicking New under the Applications button. If you want the ANSI
templates to be your default you can change this under the Appllication
button -Solid Edge Options (at the bottom) - Helpers - Set Default Templates
David
"John Beattie" wrote in message
news:49be9745$1@bbsnotes.ugs.com...
>
> There is no print option on the application menu. How do I print?
> Can't find rotate function as described in help?
> How can I change default settings so units will default to inches?