Reply

Problem with Installation

Hi,

I keep getting an error message using the Windows Installer. I get an error message telling me that the file _isF4.tmp is not in the temporary directory and needs to be installed. Then it blows me out of the Install program without finishing.

The one confusing thing during the install is that the target directory for the install is in TEMP. Shouldn't the target directory be in Program Files?

Thanks,

Tom Hess
1 REPLY

Re: Problem with Installation

I just found the answer from a post in June - you need to have .NET Framework 3.5 installed to run the SE Free 2D installer.