Reply

Profile Lines


I read the following in the help file.
"When using profile lines, any profile elements that are not part of the feature
you are constructing must be toggled to construction elements using the Construction
command on the Draw toolbar."
1. Where is the profile line type accessed? I doesn't show up in the list of line
types.
2. Where is the Construction command? It is not on the Draw toolbar as stated.
Thanks,
Ed
1 REPLY

Re: Profile Lines

Ed,
I believe this refers to using Solid Edge full 3D package.
David
"Ed Kadlec" wrote in message
news:4810c669$1@bbsnotes.ugs.com...
>
> I read the following in the help file.
>
> "When using profile lines, any profile elements that are not part of the
> feature
> you are constructing must be toggled to construction elements using the
> Construction
> command on the Draw toolbar."
>
> 1. Where is the profile line type accessed? I doesn't show up in the list
> of line
> types.
>
> 2. Where is the Construction command? It is not on the Draw toolbar as
> stated.
>
> Thanks,
> Ed