Remove "R", just have radius symbol

N/A
I cannot seem to remove the "R" in a radius dimension. I have successfully
added the radius symbol, but cannot remove the following R between the
symbol and the dimension. Any help?

5 REPLIES

Re: Remove "R", just have radius symbol

N/A
What radius symbol are you displaying?
What standard are you trying to adhere to?
Rick B.

Re: Remove "R", just have radius symbol

N/A
ISO, Ø R 123.456

Re: Remove "R", just have radius symbol

N/A
ISO, Ø R 123.456


Ø is diameter
R is radius

R = D/2 ;-)

Re: Remove "R", just have radius symbol

N/A
So the questions are:
Are you wanting a radius dimension?
Or, are you wanting a diameter dimension?
The diameter symbol 'Ø' is never displayed with a radial dimension.
The radius symbol 'R' is never displayed with a diameter dimension.
When you place the dimension, you can specify which type to create "diameter
or radial'.
You will get the proper symbol based on the type.
Regards,
Rick B.

Re: Remove "R", just have radius symbol

N/A
Yes... a blunder made possible by yours truly. Smiley Happy
"Ricky Black" wrote in message
news:4d8214d7$1@bbsnotes.ugs.com...
> So the questions are:
> Are you wanting a radius dimension?
> Or, are you wanting a diameter dimension?
>
> The diameter symbol 'Ø' is never displayed with a radial dimension.
> The radius symbol 'R' is never displayed with a diameter dimension.
>
> When you place the dimension, you can specify which type to create
> "diameter or radial'.
> You will get the proper symbol based on the type.
>
> Regards,
> Rick B.
>
>