ST9 2D Docking Toolbar

Experimenter
Experimenter

I have seen a toolbar in YouTube tutorial videos just below the main toolbar. It shows the allowable parameters for the drawing objects and data may be entered there. It doesn't disappear when the focus is on the drawing. My equivilant toolbar is on the left of the drawing and will auto-hide. I can't get it to move under the main toolbar.  Yes, I'm a rank beginner. Just started using Solid Edge today.

 

Thanks

Tom

2 REPLIES

Re: ST9 2D Docking Toolbar

Esteemed Contributor
Esteemed Contributor

Hi there @Tom4,

 

Welcome.

I think the only part you are missing, is selecting the auto-hide button.....this then means you can "grab" the title bar, dragging it out to the graphics window, will evoke the docking indicators. HTH

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP2] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: ST9 2D Docking Toolbar

Experimenter
Experimenter

Thanks Sean,

 

That helped. I also had to click the Application button/settings/Customize and select "Use horizontal command bar". Now all is as I wish.

 

Tom