Solid Edge 2D Drafting ST4 Release Soon

Siemens Phenom Siemens Phenom
Siemens Phenom
All,
I am posting this notice to let you know that Solid Edge ST4 has been released. What this means to you is that Solid Edge 2D Drafting ST4 will be released soon. If you are interested in upgrading to the latest version, please check the following link occasionally. It will specify which version is available.

http://www.plm.automation.siemens.com/en_us/products/velocity/solidedge/free2d/index.shtml

Regards,
Rick B.
14 REPLIES

Re: Solid Edge 2D Drafting ST4 Release Soon

N/A
Any idea what the changes will be?

Re: Solid Edge 2D Drafting ST4 Release Soon

Siemens Phenom Siemens Phenom
Siemens Phenom
There has been a significant amount of work done relative to global standards (ANSI ASME, ISO, ESKD, and GB). Otherwise, there are a number of bug fixes.

Regards,
Rick B.

Re: Solid Edge 2D Drafting ST4 Release Soon

N/A
ST4 is now available to download.

Re: Solid Edge 2D Drafting ST4 Release Soon

N/A
The download is for ST4 but the license file is for ST3 so the installation won't complete.

Re: Solid Edge 2D Drafting ST4 Release Soon

N/A
It installed ST4 for me with no problems.

Make sure you just download the install program and not the separate license file. The install program includes the necessary license file and will install it when you run the installation file.

Re: Solid Edge 2D Drafting ST4 Release Soon

N/A
Thank you. I will try that out.

Re: Solid Edge 2D Drafting ST4 Error

N/A
Hi,
I have just installed the new version and I get an error when starting the program:

Solid Edge License Check
A connection to the license file server could not be established.
Invalid license file syntax.
Feature: server_id
License PATH: C:\Programme\Solid Edge 2D Drafting ST4\Program\SELicense.dat
FLEXnet Licensing Error: -2,413

The previous version ST3 worked perfectly on the same setup.

Please help!

Fritz

Re: Solid Edge 2D Drafting ST4 Error

N/A
Hi,

Following Rick's advice in another thread, this is the content of my SELicense.dat file:
L À F‹ &¤¸ËÒÌÉ \ Ñ ÞÌÉ ¢ÛkpÌÌÉ / PàOÐ ê:i ¢Ø +00� /C:\ 8 3 7 ¡©Ì System C:\ . . \ . . \ . . ` *X sleipnir $@•¹@èÍO“ò©Pñ ±ƒhµÂDÑ8Þ €5 " ¡N $@•¹@èÍO“ò©Pñ ±ƒhµÂDÑ8Þ €5 " ¡N

I hope this helps to get help...Smiley Happy

Fritz

Re: Solid Edge 2D Drafting ST4 Release Soon

N/A
SE Free2d Having trouble with Licence validation **Try this Fix**


I had problems installing the new ST4 with licence validation, the answer I figured out was to
:
1: uninstall it if you have already installed ST4 2D
2: turn off User Account Control
3: Make sure your install file is on a drive on your computer, not a shared network drive
4: Right click install file "SE2DDraftV104ENGLISH.exe" and run as Administrator
5: After install and run turn on User Account Control

It work for me hope it works for

Mikew