Reply

Suddenly can't delete elements


What did I do wrong? I haven't used SE for a couple of months. Today, I was trying
to edit a drawing and I can't delete elements of a drawing. Why is that
For instance, I have SELECT highlighted, then click on the line. Normally I could
just hit the delete button on the keyboard. Suddenly that no longer works.
I muse have inadvertently changed something. Any ideas?
2 REPLIES

Re: Suddenly can't delete elements

Have you toggled off the Dimensions and Annotations option in the Select
Options Filter?
Another one to look out for in this dialogue is that the 'All Layers' option
is set instead of 'Active Layer Only'
The Select Options command is found towards the top of the Command Bar which
by default is upper left area of the screen in the ST version or on the
Ribbon bar above graphics area in earlier versions.
Jon
"Sam Hoskins" wrote in message
news:4a60d398$1@bbsnotes.ugs.com...
>
> What did I do wrong? I haven't used SE for a couple of months. Today, I
> was trying
> to edit a drawing and I can't delete elements of a drawing. Why is that
>
> For instance, I have SELECT highlighted, then click on the line. Normally
> I could
> just hit the delete button on the keyboard. Suddenly that no longer
> works.
>
> I muse have inadvertently changed something. Any ideas?


Re: Suddenly can't delete elements

Sorry meant to say Wireframe instead of Dimensions and annotations below

"Jon Sutcliffe" wrote in message
news:4a656ec7@bbsnotes.ugs.com...
> Have you toggled off the Dimensions and Annotations option in the Select
> Options Filter?
> Another one to look out for in this dialogue is that the 'All Layers'
> option is set instead of 'Active Layer Only'
> The Select Options command is found towards the top of the Command Bar
> which by default is upper left area of the screen in the ST version or on
> the Ribbon bar above graphics area in earlier versions.
>
> Jon
>
> "Sam Hoskins" wrote in message
> news:4a60d398$1@bbsnotes.ugs.com...
>>
>> What did I do wrong? I haven't used SE for a couple of months. Today, I
>> was trying
>> to edit a drawing and I can't delete elements of a drawing. Why is that
>>
>> For instance, I have SELECT highlighted, then click on the line. Normally
>> I could
>> just hit the delete button on the keyboard. Suddenly that no longer
>> works.
>>
>> I muse have inadvertently changed something. Any ideas?

>
>