Surface area only in mm2?

Experimenter
Experimenter

I have to convert surface area in Callout text from mm2 to m2.Is this posible?I was searching all day,butt coudnt find it.

2 REPLIES

Re: Surface area only in mm2?

Esteemed Contributor
Esteemed Contributor

Hi there,

 

Try, while in an active SE document, go to Solid Edge Options > Units tab.....look for the drop down to change the units for Area.

 

ST7_Draft_SE Options.png

 

ST7_Draft_SE Options_Units_Area.png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP2] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Surface area only in mm2?

Experimenter
Experimenter

Thank you for answering.I have ST6 version and there is no "Units" in Solid edge options.

But I did find it after all .It is in Properties-->file properties-->units.