Cancel
Showing results for 
Search instead for 
Did you mean: 

Transparent images -- Earlier Version of Solid Edge

N/A

Hi Ricky
Re My earlier enquiry on the transparent images. I am using V102 and would like
to go back to version 19 or a version where I am able to use the transparent function
on imported inages. I have V19 and V100 on disk. Can I install either of those
versions over the top of V102 or do I need to uninstall V102 and install V19 or
V100 or whatever works with the functioning transparent facility.
As you mentioned the transparent function will be fixed in the next version. When
will the new version be available?
Many thanks
Geoff
3 REPLIES

Re: Transparent images -- Earlier Version of Solid Edge

N/A

"Geoff Burford" wrote:
>
>Hi Ricky
>Re My earlier enquiry on the transparent images. I am using V102 and would
>like
>to go back to version 19 or a version where I am able to use the transparent
>function
>on imported inages. I have V19 and V100 on disk. Can I install either of
>those
>versions over the top of V102 or do I need to uninstall V102 and install V19
>or
>V100 or whatever works with the functioning transparent facility.
>
>As you mentioned the transparent function will be fixed in the next version.
>When
>will the new version be available?
>
>Many thanks
>Geoff

Geoff, I'm not Ricky but I'm a user of the latest version. I'm in love with it.
I haven't run into a single problem. Previously, I had all kind of problems with
making BLOCKS. I would never go back.
Good Luck,
Ron
Ronald W Latour

Re: Transparent images -- Earlier Version of Solid Edge

N/A

Hi Ron
Thanks for the reply. Yes I am also happy with the latest version. Ricky said that
the transparency problem would be fixed in the next version. I will wait for that.
It is not an urgent problem. it is just nice to be able to get a verifying result
with an overlay.
thanks
Geoff



"Ronald W Latour" wrote:


>
>"Geoff Burford" wrote:
>>
>>Hi Ricky
>>Re My earlier enquiry on the transparent images. I am using V102 and would
>>like
>>to go back to version 19 or a version where I am able to use the transparent
>>function
>>on imported inages. I have V19 and V100 on disk. Can I install either of
>>those
>>versions over the top of V102 or do I need to uninstall V102 and install

>V19
>>or
>>V100 or whatever works with the functioning transparent facility.
>>
>>As you mentioned the transparent function will be fixed in the next version.
>>When
>>will the new version be available?
>>
>>Many thanks
>>Geoff

>
>Geoff, I'm not Ricky but I'm a user of the latest version. I'm in love with
>it.
> I haven't run into a single problem. Previously, I had all kind of problems
>with
>making BLOCKS. I would never go back.
>
>Good Luck,
>Ron
>Ronald W Latour
>

Re: Transparent images -- Earlier Version of Solid Edge

N/A
Geoff,
You cannot have two versions loaded at the same time. To go back, you will
have to uninstall the current version.
Just a warning, any file saved in the current version cannot be opened on a
previous version. Files are upward compatable only.
Regards,
Rick B.