User defined table in drafting

Experimenter
Experimenter

How we can merge two cells of two adjacent column?

 

Thanks

sachin

4 REPLIES

Re: User defined table in drafting

Genius
Genius

Hey,

 

You can only merge cels in one colum if them values are the same.

SE ST9 + TC 10.1.7

Re: User defined table in drafting

Experimenter
Experimenter

Thanks for your reply...

It dont allow to merge cells if they are in one column also.

What I observed is that, if I create rows under the "Header" and not as "Data" cells, it allows me to merge in one column and with different column also.

Re: User defined table in drafting

Genius
Genius

I only use FOP Table and BOM in SE, in other case I use Excel tables.

SE ST9 + TC 10.1.7

Re: User defined table in drafting

Esteemed Contributor
Esteemed Contributor

I believe you can only merge Column Headers horizontally.  The cell data can only be merged vertically.


Thanks,
Ken

Production: ST9 MP10
Testing: ST10 MP3