Using the free Solid Edge 2D Drafting in Citrix

N/A
Hi,
We have a user that needs to use the free Solid Edge 2D drafting over a
Citrix connection. Right now if he tries to open the program he gets a
"Solid Edge 2D Drafting could not find a valid license" error. Is it
possible to use this program using Citrix? If so, how do we do it?
Thanks.

1 REPLY

Re: Using the free Solid Edge 2D Drafting in Citrix

N/A
Dan,
I don't know if I fully understand your configuration, but I will try to
offer some suggestions.
Solid Edge 2D Drafting must be installed locally, not run remotely.
Solid Edge 2D Drafting will not run along with a Citrix server. The Draft
files can be copied locally and then accessed by 2D Drafting.
In short everything must be on the local machine.
Regards,
Rick B.