Reply

V100 - THINGS I DON'T LIKE


The more I use V100, the more I don't like it. Maybe I have a faulty download and
may need to reset.
I don't like having to search for the initial email from Ricky to use that thread
for Likes and Dislikes. So I started a new one.
When I draw lines, I can't cancel the command after placing the line using ESC.
I have to select another command and than ESC. I can cancel other commands but
not lines.
I don't like it when I can't cancel a any command using the ESC key. I'm constantly
using UNDO because I didn't want to place e.g., a rectangle, so I hit ESC. The
command is interrupted but only after the first action is completed, i.e., the rectangle
is placed. I think this was true with the older version also.
I can't find the icon to turn Show Relationships. So I put on it on the QAB. But
than I can't tell whether it's activated or not.
I liked the Grid bar to show all of the time and can't figure out to do that. I
put the Grid comand on the QAB but have to turn it on each time I open SE.
When trying to reduce the font in the Prompt bar, if I click too fast, the bar moves
to someother place.
And while I'm at it, I don't like having to hit enter after selecting such commands
as Make Group. It's a pain. Yea I know this was the case with the older version.

Ronald W Latour
1 REPLY

Re: V100 - THINGS I DON'T LIKE

Ronald,
I wonder if you don't have a bigger issue. See my replies below

"Ronald W Latour" wrote in message
news:490f4152$1@bbsnotes.ugs.com...
>
> The more I use V100, the more I don't like it. Maybe I have a faulty
> download and
> may need to reset.
>
> I don't like having to search for the initial email from Ricky to use that
> thread
> for Likes and Dislikes. So I started a new one.
>
> When I draw lines, I can't cancel the command after placing the line using
> ESC.
> I have to select another command and than ESC. I can cancel other commands
> but
> not lines.

I don't see this problem. ESC works for me just fine

> I don't like it when I can't cancel a any command using the ESC key. I'm
> constantly
> using UNDO because I didn't want to place e.g., a rectangle, so I hit ESC.
> The
> command is interrupted but only after the first action is completed, i.e.,
> the rectangle
> is placed. I think this was true with the older version also.

As before, ESC works for me in every scenario you list.

> I can't find the icon to turn Show Relationships. So I put on it on the
> QAB. But
> than I can't tell whether it's activated or not.

You can tell if the command is activated by the icon back ground color. In
the attached image titled ACTIVE you will see
an orange background. Compare this to the attached image titled INACTIVE

> I liked the Grid bar to show all of the time and can't figure out to do
> that. I
> put the Grid comand on the QAB but have to turn it on each time I open SE.


> When trying to reduce the font in the Prompt bar, if I click too fast, the
> bar moves
> to someother place.

I can't duplicate this

>
> And while I'm at it, I don't like having to hit enter after selecting such
> commands
> as Make Group. It's a pain. Yea I know this was the case with the older
> version.

Choose the Accept icon or RMB to complete the command. ENTER is not
required.

> Ronald W Latour