V102 will not install

N/A
I have tried to install Solid Edge 2D several times and I keep getting the following error message. "File 'C:\Docume~1\dstewart\LOCAL~1\Temp\_isB.tmp' cannot be found. Make sure the file in on target system or installed already." With each attempt, the .tmp file name is different. Any suggestions?

Thanks
Dean Stewart
4 REPLIES

Re: V102 will not install

N/A
I have no suggestions to help but I can say that the same procedure is happening to me. I am calling in the morning to connect to some help.

Re: V102 will not install

N/A
There is a posting to this newsgroup further down in the list called;
IF 2D DRAFTING FAILS TO INSTALL - READ THIS
Everything you need to know to get past this issue is in that post.
Regards,
Rick B.

Re: V102 will not install

N/A
Can not find posting, can not install free 2d package.

Any suggestions as to how to correct the installation glitch: missing _isB.tmp file?

Re: V102 will not install

N/A
If 2D Drafting fails to install and gives an error about a '.tmp' file
cannot be found, there is a fix for the problem.
Go to the following web site and install .NET 3.5. This is a Microsoft
install.
http://www.microsoft.com/downloads/details.aspx?familyid=333325FD-AE52-4E35-B531-508D977D32A6&displa...
Simply click on the Download button on this web page.
I prefer saving the file to a specific location and then running the file
from there.
After you have installed .NET 3.5, install Solid Edge 2D Drafting again.
Regards,
Rick B.