V20 to V102

N/A
I just upgraded to V102 from V20. Is it necessary to uninstall V20 before installing V102? I now have both installed and V20 still works but V102 takes about 5 minutes to come up and it cannot open any drawings made by V20 nor can it create a new drawing. I checked the system requirements and my laptop does support SSe2 however in add/remove programs the MS C++ didn't appear. During install a message came up indicating .net 2 had not installed however add/remove showed it as being installed with all service packs.
2 REPLIES

Re: V20 to V102

N/A

Per the installation instruction given when V102 was released:
"Solid Edge detects whether you have an existing version of Solid Edge installed
and prompts you appropriately prior to installing this version. Two versions of
Solid Edge cannot be installed via Windows Installer on the same machine. Please
refer to the section "Uninstalling Solid Edge" in this README file for information
on proper uninstallation techniques."
Hope this helps.

hrwaller@yahoo.com wrote:
>
>I just upgraded to V102 from V20. Is it necessary to uninstall V20
>before installing V102? I now have both installed and V20 still works
>but V102 takes about 5 minutes to come up and it cannot open any
>drawings made by V20 nor can it create a new drawing. I checked the
>system requirements and my laptop does support SSe2 however in
>add/remove programs the MS C++ didn't appear. During install a message
>came up indicating .net 2 had not installed however add/remove showed it
>as being installed with all service packs.
>
>
>--
>hrwaller@yahoo.com
>------------------------------------------------------------------------
>hrwaller@yahoo.com's Profile: http://bbsnotes.ugs.com/vbulletin/member.php?userid=70305
>View this thread: http://bbsnotes.ugs.com/vbulletin/showthread.php?t=41324
>


Re: V20 to V102

N/A
When you tried to install V102, you should have been told that there was
already a version loaded.
Installation should have detected this and stopped.
Can you still open your files in V20?
Regards,
Rick B.