Version ST3

N/A
Ricky,
Have just downloaded Version ST3 - always a bit concerned there may be
gremlins. Operating system used is Windows 7, and following general advice
from you UAC was turned down to the minimum setting. The download was
completed in just over 7 minutes and all ran very smoothly.
On first sight the new Interface looks clearer than ST2 and first
impressions are that the software appears to be more intuitive. There was
no problem installing my own background sheets, which has been a a bit of a
pain in previous versions - in part because of my inexperience. Existing
ST2 drawings are seamlessly transferred to ST3.
Now looking forward to drawing up one or two woodworking projects.
Sincere thanks for everything,
Roger
4 REPLIES

Re: Version ST3

N/A
Is there a ST3 version of Solid Edge 2D?
I just filled out the form for SE free2D again and still got a downloadable file SE2DDraftV102ENGLISH.exe, which is the same as the ST2 that i am running now...
Where did you find the download?

Re: Version ST3

N/A
It should have given you V103.

Re: Version ST3

N/A
Good day,
Yes, there is a ST3 version. I picked up the link from Ricky Black's post
on 6th December 2010 this took me to the download page. I registered first
and then went to download - I seem to remember there was an option to
download 'licence' which is a bit confusing.
No doubt Ricky will respond to your post in more detail if there is an
issue.
Good luck.
Roger

"roelnoorman@gmail.com" wrote in message
news:roelnoormangmail.com.4no6nb@noreply.bbsnotes.ugs.com...

Is there a ST3 version of Solid Edge 2D?
I just filled out the form for SE free2D again and still got a
downloadable file SE2DDraftV102ENGLISH.exe, which is the same as the ST2
that i am running now...
Where did you find the download?

--
roelnoorman@gmail.com
------------------------------------------------------------------------
roelnoorman@gmail.com's Profile:
http://bbsnotes.ugs.com/vbulletin/member.php?userid=256800
View this thread: http://bbsnotes.ugs.com/vbulletin/showthread.php?t=44363

Re: Version ST3

N/A
ST3 is available for download.
There are a number of web sites around the globe that are being updated to
download ST3.
Some may be lagging behind and still downloading ST2.
If you want to download ST3, go to the following web site to register for
ST3.
Click on the appropriate link on the right hand of the web page to download
the latest version.
You can still select which language to download.
http://www.plm.automation.siemens.com/en_us/products/velocity/solidedge/free2d/index.shtml
Regards,
Rick B.