Vertical relationship problem in tutorial

N/A

Hi,
I've been working through the tutorials, but I'm stuck on the bit where I line up
the two drawings using vertical relationships. Every time I click on any line with
the vertical/horizontal relationship tool I get a message saying "The requested
change conflicts with existing relationships".
Any suggestions?
5 REPLIES

Re: Vertical relationship problem in tutorial

N/A

Tom,
Can you send us your file so we can look at it?
Ed
"Tom C" wrote:
>
>Hi,
>I've been working through the tutorials, but I'm stuck on the bit where I
>line up
>the two drawings using vertical relationships. Every time I click on any line
>with
>the vertical/horizontal relationship tool I get a message saying "The requested
>change conflicts with existing relationships".
>
>Any suggestions?

Re: Vertical relationship problem in tutorial

N/A
Hi,
I'm having a similar issue, and I have red through a few other threads, but not worked it out yet. Any help would be appreciated. t
I am struggling also to upload the file, The uploaded has stalled?

Sean

Re: Vertical relationship problem in tutorial

Esteemed Contributor
Esteemed Contributor
If you pick a line with the command and do not select a keypoint (endpoints or midpoint), it will attempt to make the line horizontal/vertical and will not allow a second point to be picked.
Sent from my Kindle Fire using Tapatalk 2

Thanks,
Ken

Production: ST9 MP10
Testing: ST10 MP3

Re: Vertical relationship problem in tutorial

N/A
...can you please lead me to the tutorials. I would like to learn more about Solid Edge 2D, but I am having a hard time finding lessons/tutorials. thank you in advance

Re: Vertical relationship problem in tutorial

N/A
...can you please lead me to the tutorials. I would like to learn more about Solid Edge 2D, but I am having a hard time finding lessons/tutorials. thank you in advance


On the SE start page click on "View all Solid Edge tutorials...". See attached image.

Hope this helps.