bolt hole circle

N/A

you say that this command is for existing bolt hole circles, what if I need to create
a bolt hole circle
2 REPLIES

Re: bolt hole circle

N/A
Ed,
You can create a circle that will become the diameter of the bolt hole
circle. Then draw circles with theri centers attached to this circle. then
place angular dimensions between the circles for position.
Further down in the list of topics there is a thread called "Bolt Hole
Circle". Open that thread. I have posted an example.
Regards,
Rick B.

Re: bolt hole circle

N/A

"Ricky Black" wrote:
>Ed,
>You can create a circle that will become the diameter of the bolt hole
>circle. Then draw circles with theri centers attached to this circle. then
>
>place angular dimensions between the circles for position.
>
>Further down in the list of topics there is a thread called "Bolt Hole
>Circle". Open that thread. I have posted an example.
>
>Regards,
>Rick B.
>
>

If this program worked properly the bolt hole circle creator should do all this
for you. the bolt hole circle creator works fine in version 20 why doesnt if work
in this program. you say this is a fully functional drafting progam.