Reply

cannot show circle command bar


I am working my way through the tutorial again, and it indicates when drawing a circle
their will be a command bar in which I can specify the diameter. I cannot get the
command bar to be visible. I can use properties to set the diameter- but this takes
several steps. Suggestions? I am using the most recent version.
Thanks for any assistance.
Jeff Thiele
1 REPLY

Re: cannot show circle command bar


Jeff,
See attached image. That is what you should be seeing.
Ed
"Jeff Thiele" wrote:
>
>I am working my way through the tutorial again, and it indicates when drawing
>a circle
>their will be a command bar in which I can specify the diameter. I cannot
>get the
>command bar to be visible. I can use properties to set the diameter- but
>this takes
>several steps. Suggestions? I am using the most recent version.
>
>Thanks for any assistance.
>Jeff Thiele