Reply

how to complete this free download

hi
i have downloaded solid edge and the viewer on to my new computer and then i followed the prompt to download a licence which i now have, but the licence wont open in the viewer and i'm not sure what to do next as solid edge won't open.
hope you can help
thanks jeff
5 REPLIES

Re: how to complete this free download

When you download the Solid Edge 2D Drafting, there is no need to download a
license.
You also do not need to download the viewer. It is included with 2D Drafting
as a single installation.
The download is an installation executable. It can be saved and run at any
time.
I suggest that you save the file when prompted instead of running.
This way you have the executable if you need to install the software again.
After it is saved to your machine, it will ask if you wnat to run at that
time.
Uninstall both Solid Edge 2D Drafting and/or the free viewer.
Install 2D Drafting again.
If you need to return to the web site and register again to get the
download, that is OK.
Before you attempt tto install the software, check the following.
Make sure you have administrator priveleges.
If you are running Vista or Windows 7, make sure you have the UAC (User
Account Control) turned off.
After installing the software, you can reset it.
Regards,
Rick B.
"jeffreyknight@btinternet.com"
wrote in
message news:jeffreyknightbtinternet.com.4rn4pn@noreply.bbsnotes.ugs.com...
>
> hi
> i have downloaded solid edge and the viewer on to my new computer and
> then i followed the prompt to download a licence which i now have, but
> the licence wont open in the viewer and i'm not sure what to do next as
> solid edge won't open.
> hope you can help
> thanks jeff
>
>
> --
> jeffreyknight@btinternet.com
> ------------------------------------------------------------------------
> jeffreyknight@btinternet.com's Profile:
> http://bbsnotes.ugs.com/vbulletin/member.php?userid=320666
> View this thread: http://bbsnotes.ugs.com/vbulletin/showthread.php?t=45133
>


Re: How large is this program?

How lare is this program?

Re: How large is this program?

How large is this program?

Re: how to complete this free download

thank you for your help

Re: how to complete this free download

The download is 400+MB.