installation Vista OS

N/A

I tried several time to install SE2DDRAFT on VISTA PRO but at the end of the installation
session, i got this error message:
microsoft.vc80.ATL, type="win32", version="8.0.50727.762", publickeyToken="1fc8b3b9a1e18e3b",process
or architecture=x86"
Somebody, can help me?
Thanks a lot for answering.
2 REPLIES

Re: installation Vista OS

N/A
Grandjean,
This looks like a Microsoft error. We use some Microsoft components during
installation.
I suggest you go to the Microsoft web site and search for this error. I did
this and found the following.


I started with this error and then my IT guy found out it was due to a
problem with Windows Update. Lo and behold, when I checked on windows
update, it had failed nearly every attempted download/installation. You
need to install service pack 1 separately. After that, you can install
Itunes. If you have trouble fixing windows update, like I did, try these
two methods below (I did them both at the same time )

http://www.windowsreference.com/windows-vista/fix-for-vista-sp1-install-error-80073712-through-windo...

http://windowshelp.microsoft.com/Windows/en-US/Help/ca7d15d7-8ee3-4993-bd01-753dadc904121033.mspx


Hope this helps.
Regards,
Rick B.


Re: installation Vista OS

N/A

I made the second proposal, then tried the installation process. And all is well
this time. I have installed the software on my computer.
Thanks a lot for your help.
Regards
Xavier
"Ricky Black" wrote:
>Grandjean,
>This looks like a Microsoft error. We use some Microsoft components during
>
>installation.
>I suggest you go to the Microsoft web site and search for this error. I did
>
>this and found the following.
>
>
>
>
>I started with this error and then my IT guy found out it was due to a
>problem with Windows Update. Lo and behold, when I checked on windows
>update, it had failed nearly every attempted download/installation. You
>need to install service pack 1 separately. After that, you can install
>Itunes. If you have trouble fixing windows update, like I did, try these
>
>two methods below (I did them both at the same time )
>
>
>http://www.windowsreference.com/windows-vista/fix-for-vista-sp1-install-error-80073712-through-windo...
>
>
>http://windowshelp.microsoft.com/Windows/en-US/Help/ca7d15d7-8ee3-4993-bd01-753dadc904121033.mspx
>
>
>
>
>
>Hope this helps.
>Regards,
>Rick B.
>
>
>