cancel
Showing results for 
Search instead for 
Did you mean: 

[langtitle=de]Ich kann Solid Edge 2 nicht starten[/langtitle]

N/A
Ich habe soeben ie Software installiert.
Beim versuch das Programm zu starten kommt die Meldung
"keine gültige Lizenz gefunden".

Einte Lizenzdatei habe ich bekommen und in das Verzeichnis kopiert in dem Solid edge eingerichtet wurde...dort dann auch in der Unterverzeichnis "programm files".

Wer kann mir weiter helfen?

Danke Manni P
16 REPLIES

Re: [langtitle=de]Ich kann Solid Edge 2 nicht starten[/langtitle]

N/A
Danke,
This sounds like a problem that a few others are having.
The issue is that there are files in your system folders with future dates.
Solid Edge 2D Drafting uses a timed license which is renuable for free.
We do this to try to keep everyone up to date on new releases.
The license software checks system files to see if any files have dates in
the future relative to the system date.
If this is the case, it invalidates the license.
Regards,
Rick B.

Re: [langtitle=de]Ich kann Solid Edge 2 nicht starten[/langtitle]

N/A
I´m having the same problem, what should i do to fix it????
thanks

Re: [langtitle=de]Ich kann Solid Edge 2 nicht starten[/langtitle]

N/A
Have you verified that is is a problem with system file dates?
I can send some simple directions to create a dump of your system files.
It creates a text file that you can look through for dates.
Regards,
Rick B.

Re: [langtitle=de]Ich kann Solid Edge 2 nicht starten[/langtitle]

N/A
Î have a problem with this programm. I cant drawing with this. Why? P.S I am from germany

Re: [langtitle=de]Ich kann Solid Edge 2 nicht starten[/langtitle]

N/A
Can you create a new drawing file or does the software not run at all?
Rick B.

Re: [langtitle=de]Ich kann Solid Edge 2 nicht starten[/langtitle]

N/A
Have you verified that is is a problem with system file dates?
I can send some simple directions to create a dump of your system files.
It creates a text file that you can look through for dates.

Regards,
Rick B.


Which is the folder that Solid Edge 2 checks as I found quite some future timestamps on my system

Regards,
Peter

Re: [langtitle=de]Ich kann Solid Edge 2 nicht starten[/langtitle]

N/A
Peter,
It will be any folder including and under the 'C:\windows' folder.
You can create a dump of the folder structure by doing the following.
This will help find the files with future dates.
You can look at thedates that are generated in the file created by the
following.
This is a tediuos process, but is better than clicking through each folder.
Once the system date catches up with the most future file date, 2D Drafting
will start working again.
Click on Start and then Run.
In the 'Open' field key in cmd.
This opens a command window.
key in 'cd c:\windows' without the qotes.
key in 'dir *.* /s >C:\WinDirectoryContent.txt' without the quotes.
Wait until you get the prompt back.
This will create a file called 'WinDirectiryContent.txt' at the 'c:\' root
folder.
key in 'c:\' without the quotes.
key in 'dir *.txt' without the quotes.
You should see a file 'WinDirectoryContent.txt'.

Make sure the file is not empty.
Regards,
Rick B.

Re: [langtitle=de]Ich kann Solid Edge 2 nicht starten[/langtitle]

N/A
Peter,
It will be any folder including and under the 'C:\windows' folder.

You can create a dump of the folder structure by doing the following.
This will help find the files with future dates.
You can look at thedates that are generated in the file created by the
following.
This is a tediuos process, but is better than clicking through each folder.

Once the system date catches up with the most future file date, 2D Drafting
will start working again.

Click on Start and then Run.

In the 'Open' field key in cmd.

This opens a command window.

key in 'cd c:\windows' without the qotes.

key in 'dir *.* /s >C:\WinDirectoryContent.txt' without the quotes.

Wait until you get the prompt back.

This will create a file called 'WinDirectiryContent.txt' at the 'c:\' root
folder.

key in 'c:\' without the quotes.

key in 'dir *.txt' without the quotes.

You should see a file 'WinDirectoryContent.txt'.


Make sure the file is not empty.

Regards,
Rick B.


Thanks Rick,

I found 154 files and 38 directories dated 2020 in the sub directories of windows and some of them are used by the system as well.
Does that mean that I have to check each individual file and folder now and try to correct the date of this files and folders?

Regards,
Peter

Re: [langtitle=de]Ich kann Solid Edge 2 nicht starten[/langtitle]

N/A
how to download solid edge v19