Reply

layer color? and properties?

Can I assign a colors by layer? If I try to set layer properties I get a
blank window, with no hit of what possible properties there are to assign.
Couldn't find anything in help either. What are the layer properties, and
is color one of them?
thanks,
--steve

1 REPLY

Re: layer color? and properties?

Steve,
The properties on Layers are used to add user defined data to the layer. In
Solid Edge this data can be accessed by macros that the user writes such as
in Visual Basic.
Layers do not have color overrides as they do in AutoCAD. All a layer will
do is control Show/Hide of the objects assigned to the layer.
Regards,
Rick B.