Cancel
Showing results for 
Search instead for 
Did you mean: 

offsetting lines without dimensions as well as more tutorials

N/A

hi guys, I am a newbie with regards to this program. only downloaded it yesterday.
two questions for today, how do I ofset lines without having the dimensions crop
up every time, as well as, where are more tutorials or manuals for the program.
Thanks and regards
Thys
1 REPLY

Re: offsetting lines without dimensions as well as more tutorials

N/A
Thys,
The dimension placed with the Offset command is the driving constraint that
defines the offset distance. If you do not want the dimension, delete it.
Use help to search for topics of interest.
There are three tutorials delivered with the product.
Regards,
Rick B.