Reply

program wont run once loaded


Can anyone help,i downloaded the program from the cd and got the licence and changed
it to the .dat as was explained and also put it into the correct file, when i go
to start the program it says i have no licence key, what gives????, tried to get
hold of the support people at ugs but i may as well be talking to a pencil, actually
i would probably get more info from a pencil, just about ready to put the ugs cd
in a trap and blast it with my shotgun, pretty darn useless program i feel and obviously
not the only person to run into such difficulties
1 REPLY

Re: program wont run once loaded

If you had other Solid Edge related software such as the free viewer, it
will cause an error and therefore must be removed. You also need to make
sure the license file was not malformed by your e-mail client. It should
have the following lines with the exception of the license code string which
I changed to X's. Never use Wordpad to edit text files, use Notepad
instead, as Wordpad inserts binary characters for formatting.
INCREMENT solidedge2ddrafting sedemon 19.0 30-sep-2007 uncounted \
XXXXXXXXXXXX HOSTID=DEMO
--
Ken
http://grundey.blogspot.com
"Glenn" wrote in message
news:458cad03$1@bbsnotes.ugs.com...
>
> Can anyone help,i downloaded the program from the cd and got the licence
> and changed
> it to the .dat as was explained and also put it into the correct file,
> when i go
> to start the program it says i have no licence key, what gives????, tried
> to get
> hold of the support people at ugs but i may as well be talking to a
> pencil, actually
> i would probably get more info from a pencil, just about ready to put the
> ugs cd
> in a trap and blast it with my shotgun, pretty darn useless program i feel
> and obviously
> not the only person to run into such difficulties