"Hide everywhere" freezes application ST7

Valued Contributor
Valued Contributor

Hi Guys

My file has a model and eight drawing sheets.

I go to the layers tab and right click a layer, then choose "hide everywhere"

Solidedge 2d shows as "not responding" in task manager

Solidedge shows a round rotating cursor and hangs for a few minutes after which it comes good and the layers are hidden.

Is this machine related or a solidedge thing?

 

Pete

 

3 REPLIES

Re: "Hide everywhere" freezes application ST7

Esteemed Contributor
Esteemed Contributor

Hi Pete,

 

Not seeing this here, show & hide as expected.......the cause could be either, or or even a combination of what you suggest. Would need more info about the circumstances under which the freeze occurs.

Are you able to share the draft file?

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP2] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: "Hide everywhere" freezes application ST7

my guess is that it's file specfic not PC nor SE.

 

Try hiding each layer everywhere 1 at a time...

 

I suspect you will find one layer that is causing the tax on the system.

 

I suspect that layer may benifit from being cleaned up...  i suspect lots of very small and overlapping entities.

 

Just a guess...  but i think worth giving a shot.

 

Re: "Hide everywhere" freezes application ST7

Valued Contributor
Valued Contributor

Hi Matt

You are correct

The layers in question were imported ACAD layers. Other layers worked as expected.

Cheers

Pete