Reply

"NEXT" button on Tutorial Window odes not appear.


The "next" button does not appear on the Tutorial dialog. I running XP SP2 with
IE7. I assume this is a problem caused by IE7. My screen is set at 1440 x 900.
See the attached screen print.
Thanks
1 REPLY

Re: "NEXT" button on Tutorial Window odes not appear.

Mitchel,
This is an intermittent problem during setup. From time to time customers
report this symptom.
What's happening is that hhactivex.dll does not get properly registered. I
don't know all the ins and outs of Setup, but setup shecks to see if you
have the file and if not, setup installs and registers it. Setup failed to
register it properly.
When customers report this problem, they have fixed it running "regsvr32
c:\windows\system32\hhactivex.dll" from a command line.
Click on Start
Click on Run
Copy and pase the following in the combo box.
regsvr32 c:\windows\system32\hhactivex.dll
Click on OK.
It should work properly now.
Regards,
Rick B.