Reply

savind as a dxf


I WAS WONDERING IF THERE IS A WAY TO SAVE THE DRAWING IN A DXF WITHOUT SAVING THE
BOARDER...I WANT TO USE THE SOFTWARE TO DRAFT BRACKETS AND SUCH AND CONVERT THE
BRACKETS INTO DXF FILES SO I MAY USE THESE FILES ON MY CNC PLASMA TABLE..
1 REPLY

Re: savind as a dxf

Dennis,
When you specify '.dxf' as the file type to save, the Options button at the
bottom of the Save As dialog will be enabled. Click on this button. This is
a Wizard that lets you customize the translation of the .dxf file. In the
first page there is an option, 'Translate background sheet on export'.
Uncheck this option. Click on the Finish button. Give your custom
configuration file a unique name. Save the .DXF file. The border should not
translate.
Regards,
Rick B.