Reply

set up


how do i set up to draw in large dem. i.e. 24'x36'?
how to draw in scale 1/4" to 1'
thanks,mark
1 REPLY

Re: set up

Mark,
You specify different working sheet sizes with Sheet Setup. Right mouse
click on the sheet tab (Sheet1) at the bottom and click on Sheet Setup.
If you need to create scaled drawings, read about 2D Model Views and Drawing
Area Setup in help. These are two different workflows for creating scaled
drawings. You always draw the geometry in Solid Edge at 1:1 scale. This way
you do not have to worry with scale as you draw. You use the tools mentioned
above to scale the drawing, not the geometry.
Regards,
Rick B.