Error on install

N/A
Hi,

I get this error trying to install on x64 Windows 8

Solid Edge 5T5 Installer Information
Error 1935.An error occurred during the installation of
assembly component
{97F81AF1-0E47-DC9O-AO1FC8B3BOA1E1SE}. HRESULT:
Ox8007O54F.

can you help.

thanks

Mark
3 REPLIES

Re: Error on install

N/A
re installed VC++ 2005, and re started install..

Re: Error on install

Pioneer
Pioneer
Sorry, but ST5 is not supported on Windows 8.
It is supported on Windows 7 Ultimate, Enterprise or Professional with SP1
Vista Business or Enterprise with SP2
Internet Explorer 9 (IE 7.0 as a minumum)

Re: Error on install

Pioneer
Pioneer
With that being said... it should still install on Windows 8 OS. This issue is most commonly seen when person installing is not administrator. Do a cleanup of registries, reboot, right mouse click in setup.exe and run as administrator installing to a location like C:\Solid Edge instead of under program files. There are some known issues with loading ST5 on a Windows 8 machine in the default location. ST6 will fully support Windows 8 which will be released later this year.