Reply

Is there a license limitation for the trial?

Hi,

 

I just installed the Sold Edge trial (says Premium in the about screen). I would like to open an existing .par file of someone else, also created in Solid Edge, and I get the error:

 

"The file you are attempting to acces was last saved in a format that is not compatible with the Solid Edge product you are using."

 

Any ideas?

 

Thanks,

Erwin

2 REPLIES

Re: Is there a license limitation for the trial?

[ Edited ]

Erwin,

 

It's a 45 Day Trial... so it doesn't appear to be the Trial issue.

 

But if the "other" person's  Part was done using a FREE Student Addition, then you may get this error.

 

Bob

Re: Is there a license limitation for the trial?

Thanks Bob, I will check if this is the case.
Erwin