Performance

Experimenter
Experimenter

I have just installed and started using the trial version.  The program is extremely sluggish and almost impossible to use properly.  I have tried to turn off just about all of the graphics enhancements possible, but it has almost no effect.  The program is even slow on selecting menu items.

 

I am running on a Dell T 7400 workstation with dual 3 GHz Xeon processors and  Windows 7 Professional operating system.  The machine has 16 GB ram and 1 TB disks.  It is an older machine, but it should in no way have problems running this program.  The system has a mid-range Nvidia graphics card installed.

 

Can anyone advise on what else can be done other than turning off the fancy graphics or what the causes of this sluggishness might be please?

 

Thank you in advance.

1 REPLY

Re: Performance

Esteemed Contributor
Esteemed Contributor

Are you using the FRA.ME cloud delivered trial version (runs in web browser)?  If so, then it has nothing to do with your PC and everything to do with your internet bandwidth/latency and the distance to the cloud server.


Thanks,
Ken

Production: ST9 MP10
Testing: ST10 MP3