cannot remove read only attributes from model

N/A
Even though I saved part with a different name and location, when trying to modify part this error occurs "The following components are read only and cannot be modified - C:\Program Files (x86)\Solid Edge ST5\Training\Frame1.par - deselect these components and rerun the edit command".
The file location is not where the part is located, and when I opened the same part in "C:\Program Files (x86)\Solid Edge ST5\Training\Frame1.par" there are no read only attributes listed to uncheck?
Windows 7 x64
I have done this operation approx 4 times with the same result.

John Tietjen
1 REPLY

Re: cannot remove read only attributes from model

Esteemed Contributor
Esteemed Contributor
By default on Windows 7, folder under Program Files (x86) are 'read only'. Being that the part is called 'Frame1.par', could it be a frame cross section that it is referring to?
Opening the part in Revision Manager (View&Markup, use the pulldown menu on the side of the Open button) to see what it may be linked to...

Thanks,
Ken

Production: ST9 MP10
Testing: ST10 MP3