Reply

looking for software that works

hei i am looking to get busy in the world of digital drawing programs.
at this time looking around in the world of cad.
solid edge looks not to be working for me i only get failure codes from it.
running win vista sp 2 whit all the specs.
any idea from some body, is this program always so problematic?

cheers Remko
4 REPLIES

Re: looking for software that works

While Windows 7 is recommended, Windows 7 Enterprise, Ultimate, or Professional (32-bit or 64-bit) with Service Pack 1 or Windows Vista Business or Vista Enterprise (32-bit or 64-bit) with Service Pack 2 (SP1 minimum) is the minimum system requirement...
Which version of Vista are you running? Also, what graphics card and driver version are you running and how much memory do you have installed?
Ken Grundey
Production: ST9 MP6
Testing: ST10

Re: looking for software that works

You'd need to be more specific about the errors you are receiving.

Did you download it from the 45day trial site?
When did you download it -- is it V104 or V105?
Did you then activate it?
What errors specifically did you receive?

Thanks,
Dan

Re: looking for software that works

I'm using WIN7 Home with service pack 1. May I install the Solid Edge trial version?
I have downloaded the "SolidEdgeV105ENGLISH_32Bit.exe and the trial licence file. But, I can't finish installation with message "The wizard was interrupted before Solid Edge ST5 could be completely installed. ... "

Re: looking for software that works

Not sure, but guessing the "Home" edition may be the issue. Perhaps it is missing something important the install needs.