Cancel
Showing results for 
Search instead for 
Did you mean: 

101 Uses of the Control and Shift Keys in Solid Edge - Part 1

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

 

 

When using the Shift and Control keys we tend to be creatures of habit. Often, there are a bunch of objects to be selected and we unknowingly press one of these keys. It could be files and folders in Windows Explorer or simply multiple items in a list box.

 

Solid Edge takes this to the next level where the Shift and Control keys when used individually and in combination with the mouse bring a large number of powerful features to your fingertips.

 

Selection in the Pathfinder

 

The foremost is the Pathfinder where the Shift key can be used to pick contiguous features. Click the first part in the list, then hold down the Shift key and select the last part in the list. The Ctrl key can be used similarly for non-sequential multiple features.

 

A potential use for this could be the Assembly PathFinder where you can use the Ctrl key to pick just a few components and start the Assembly Relationship Manager or A.R.M. which then shows the relationships for just the selected components instead of the entire assembly.

 

This is no doubt some smart behavior on part of the A.R.M. but using the Shift or Ctrl keys is the key here. No pun intended! The following video demonstrates the process.

 

It goes without saying, this technique can be used in the Part or Sheetmetal PathFinders as well.

 

 

Edge and Face Selection

 

When selecting edges or faces in a Solid Edge command, you can press the Shift or Ctrl keys to add to or remove from an existing selection, besides changing and restoring views, toggling the modeling mode, selecting multiple regions in synchronous all of which are demonstrated in this video:

 

 

TipIcon.png The above video shows that in the synchronous mode, Shift needs to be pressed only once to add the first object after which the add remove mode is ON and more edges/faces can be added to or removed from the current selection without keeping the Shift key pressed.

 

View Manipulation

 

Scroll wheel press-and-drag rotates the view SSE17.png

 

Keep the Shift key pressed and press-and-drag the wheel to Pan SSE18.png

 

Keep the Control key pressed and press-and-drag the wheel to zoom SSE16.png in a much smoother way as opposed to the jerky or incremental zoom with each tick of the scroll wheel.

 

Keep the Alt key pressed and press-and-drag the wheel to start the Zoom Area SSE19.png command.

 

Additionally keeping the Control key pressed allows zooming in an area centered around the drag start point.

 

The differences are illustrated below:

 

CSSE09.png

Did you know that in Solid Edge you can manipulate views i.e. pan, zoom and rotate all using just the keyboard?

A combination of the arrows keys, the Shift and Control keys makes this possible.

 

Arrow Keys = View Rotate

Shift + Arrow Keys = View Rotate about another axis

Ctrl + Arrow Keys = Zoom

Ctrl + Shift + Arrow Keys = Pan

 

The Zoom Fit command behaves differently when used in combination with the Shift and Control Keys.

 

Fit = Both Background Sheet and Drawing Objects

Shift + Fit = Only Drawing Objects and no concern for the Background Sheet

Ctrl + Fit = Only the Background Sheet

 

All the above techniques are illustrated in this video:

 

 

Perspective in a Jiffy

 

The View Overrides dialog on the View tab of the ribbon allows for a perspective view of the model with only 3 fixed settings, keeping the Ctrl + Shift pressed and scroll the wheel on the mouse to change the perspective of the model allows 12 values. 

 

CSSE02.png

 

 

Hip-Tip: Drawing View Power Update

 

TipIcon.png  If you hold Ctrl+Shift when you click Update Views CSSE10.png Solid Edge performs a full update, just as it would on initial view creation.  That is, it re-reads all of the model data to regenerate the view, rather than only the model data thought to have changed.

 

Universal Commands

 

Solid Edge supports all standard keyboard accelerators that use the Control key like:

 

Ctrl + N for New

Ctrl + O for Open

Ctrl + S for Save

Ctrl + P for Print

Ctrl + Z for Undo

Ctrl + Y for Redo

Ctrl + A for Select All, in Draft and Sketcher

 

Create New Keyboard Shortcuts

 

Any keyboard shortcut which is standard in your other favorite program, for example, Ctrl + W for closing a file, and is not supported by Solid Edge can be easily added using the Customize dialog as shown in the video below. The video begins with a handy shortcut Ctrl + Tab to cycle through all open docs and Ctrl + Shift + Tab to reverse the direction:

 

 

 

Standard Views

 

Sold Edge's Control+First Letter system is perhaps the simple and the most elegant of all CAD programs for switching to standard views and are listed below:

 

Ctrl + I for Isometric

 

Ctrl + T for Top

Ctrl + B for Bottom

 

Ctrl + R for Right

Ctrl + L for Left

 

Ctrl + F for Front

Ctrl + K for Back

 

Ctrl + J for Dimetric

Ctrl + M for Trimetric

 

 

CSSE04.png

 

 

More Tip and Tricks

 

Some miscellaneous uses of the Control and shift keys in lesser used commands are:

  1. Keeping the Shift key pressed when drawing a rectangle turns it into a square.
  2. Same with box command, but this does not apply when specifying the height.
  3. When drawing a line, keeping the shift key pressed, increments the angle in steps of 15°
  4. When inspecting the area of closed regions, keeping the Shift key pressed additionally displays the total area.
  5. When applying a Smart Dimension to an inclined line, the Shift key allows toggling between horizontal, vertical and aligned dimensions.

 

All these techniques can be seen in action in the following video:

 

 

 

Selection Manager

 

Pressing Shift + Spacebar starts the Selection Manager mode in the synchronous environment. This reveals a menu with over a dozen methods to intelligently select faces and features in imported models.

 

CSSE06.png

 

The video below illustrates several methods from the menu above.

 

LoudSpeaker.png Note: This video has a voice-over.

 

 

More tips...

More tricks...

More videos...

 

For more videos tip about the Shift and Control keys in Solid Edge, go to part 2 of this article...

 

 

Tushar Suradkar

www.CADVertex.com

www.SurfAndCode.IN

 

Solid Edge User Group on FaceBook:

https://www.facebook.com/groups/solidedgeusers/

Comments
Gears Phenom

Great collection! Thnx for it!