Cancel
Showing results for 
Search instead for 
Did you mean: 

3D Rendering Tutorial: How to Create Internal Lighting (Solid Edge and KeyShot)

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

When creating a 3D rendering in Solid Edge, how do you create internal lighting? I was recently asked by a colleague how to go about adding an interior emitting light INSIDE of a model in KeyShot. For example, how do you add a light to the inside of a solid cube of glass? Here's how.

 

First, model the cube in Solid Edge. In theory, instead of a cube, this could be any solid model you wish to use to emit light from. Using the KeyShot options, set the slider for the Highest Quality and the desired output size.

 

3D-Rendering-Tutorial-Cube.png

 

Note: currently in academic versions of the software, you are limited to 800 x 600 output regardless of this

Send the model to KeyShot by clicking  the KeyShot render button.

3D-Rendering-Tutorial-Render-Button.png

 

From the material Library, drag a glass material onto your part.

3D-Rendering-Tutorial-Glass-Material.png

 

From the Add Geometry fly-out in the Edit tab, add a Ground Plane. This is best to reflect the illuminating light and the shadows.

3D-Rendering-Tutorial-Ground-Plane.png3D-Rendering-Tutorial-Cube-2.png

 

Add a lighting environment from the Library. It is always a good habit to add perspective to the model to make it look more realistic.

3D-Rendering-Tutorial-Lighting.png3D-Rendering-Tutorial-Perspective.png

 

Next, we need to add an object to which to assign a light source. From the Add Geometry fly-out in the Edit tab, add a Sphere to the scene. (CTRL+5)

3D-Rendering-Add-Sphere.png

 

This adds an entry in the Project pane in the Scene tree. The sphere is huge and will obscure your scene initially.

3D-Rendering-Entry.png3D-Rendering-Huge-Sphere.png

 

Select the Sphere entry in the Scene tree, and on the Position Tab in the lower pane, drag the Scale slider to the left to make it small enough to fit inside the part.

3D-Rendering-Scene-Tree.png3D-Rendering-Scale-Slider.png

 

Select the Move Tool command and then using the arrows, drag the Sphere object inside of your part. Once inside, click the green checkmark.

3D-Rendering-Drag-Sphere.png3D-Rendering-Click-OK.png

 

Next, assign a Light material to the Sphere. There are several to choose from and you can experiment to see which one gives you the effect you want. Drag the desired light type onto the Sphere object in the Scene tree.

3D-Rendering-Area-Light.PNG3D-Rendering-Light-Type.png

 

Using the Area light, you can choose whether you want the camera to see the physical light (sphere) or just the affects of the light. To hide the source, double click on the pSphere1 entry in the Scene tree to edit the light properties.

3D-Rendering-Hide-Source.png

 

Uncheck “Visible to Camera” and “Visible in Reflections”.

3D-Rendering-Reflections.PNG

 

You can change the Power scale to Watt.

3D-Rendering-Power.png

 

If you assign a Point Light, the Sphere is automatically hidden from the camera. 3D-Rendering-Point-Light.png3D-Rendering-Point-Light-1.pngThere is no option to hide or show to the camera.

 

3D-Rendering-Point-Light-2.png

 

Adding a Spot Light gives another effect.

3D-Rendering-Spot-Light.png

 

The Move Tool on the Sphere object can be used to change the position or rotation.

3D-Rendering-Spot-Light-1.png3D-Rendering-Spot-Light-2.png,
3D-Rendering-Spot-Light-3.png

 

In this scene I added a Sphere object, hidden from the camera, to create an interior light in this assembly model.

3D-Rendering-Interior-Light.png