Cancel
Showing results for 
Search instead for 
Did you mean: 

Alternate Reality: 51 uses of the ALT key in Solid Edge

Gears Phenom Gears Phenom
Gears Phenom

This post is one of the topics suggested by Matt in Got a Story to Tell? Get Into SEU14 for Free! and discusses the many uses of the Alt key in Solid Edge.

 

Straight off the bat the first use that comes to mind is Alt + RMB for View Fit.

which is used frequently in conjunction with Alt + RMB Drag used for Zoom Area.

 

Working from memory further, in the Draft environment, Alt + Click on a callout or leader to add any number of extra vertices. Vertices are edit points that can be used to manipulate the leader line for e.g. creating a jog, etc.

 

01.png

 

Also Alt + Click on a curve in the Draft or the Sketcher to add or remove Edit Points on the curve.

 

Annotations can be associative or non-associative. An associative annotation moves when the element it is connected to moves. Make a connected annotation non-associative by pressing the Alt key while dragging the terminator handle off the element

 

Alternatively (no pun intended) move a leader line connection point to free space or to another element yet retaining associativity with the first element, by pressing the Alt+Ctrl keys while dragging the terminator handle.

 

When placing a Smart Dimension, keeping the Alt key pressed changes the appearance of the dimension. For e,g, the arc extends when placing the radius dimension.

 

02.png

 

Jogs can be added on projection lines of linear dimension using the Alt + Click.

 

04.png

 

Use Alt + Click to add one or more jogs to a selected coordinate dimension as below:

 

03.png

 

Alt + Click a dimension value to suppress the display of the dimension value edit box.

 

Count = 10

 

Conversely, Alt+Clicking anywhere on a dimension will bring up the dimension value edit box saving the hassle of aiming the mouse pointer at the text. This applies to PMI and also to dimensions in the Sketcher and Draft environments.

 

In the Draft environment, click the Select tool and Alt + Click to create a polygon fence around elements for selection.

 

05.png

 

Use Alt+drag to detach a PMI dimension or annotation from one model element and attach it to a different model element.

 

06.png

 

When a feature to which a dimension is added is deleted or suppressed, the dimension is orphaned and dangles as indicated with a brown color. Alt + Drag the handle for the extension line and drop it on to a edge or point to bring it back to life.

 

07.png

 

The grid helps drawing and modifying elements relative to known positions in the working window. Alt+X displays the X and Y coordinate input boxes, with the cursor in the X box while Alt+Y displays the X and Y coordinate input boxes, with the cursor in the Y box.
 

08.png

 

In wire harness, the path is a curve but the Alt key provides more options to the path than a simple curve in the Sketcher or Draft.

 

Alt + Click the location along the path where to add a point along the path.

 

09.png

 

To add a point to the end of the path, Alt + Click a location in free space where you want to add the point.

 

10.png

 

Alt + Click a point on the path to remove the point. When edit points are removed, the control vertex points move and the shape of the path changes. This holds true for points on a curve created using the Keypoint Curve command in the sketcher and simply the Curve command in the draft environment too.

 

11.png

 

Count = 20

 

With annotation alignment shapes, disconnect an annotation from an alignment shape by pressing Alt and then selecting the annotation border. Re-attach it by dragging the annotation on to the shape. And jogs can also be createdon the alignment line using Alt+Click.

 

12.png

 

A quick way to set the center of rotation during view rotation is to press the middle mouse button and select a point or face to set the point about which to rotate the model.

Press the Alt key while selecting the middle mouse button to cancel.

13.png

 

IntelliSketch does not recognize any relationships while holding the Alt key.
Release the Alt key to re-activate IntelliSketch.

 

In a Fastener System balloon stack, edit individual balloons in the stack by pressing the Alt key while locating and click the first balloon to modify.

 

14.png

 

Add or modify the prefix and suffix text of one or more balloons in a fastener system balloon stack by first selecting the stack and then pressing Alt while selecting the balloon to edit.

15.png

 

For Centerlines,  Alt + Drag the center line handle to detach and also to re-attach it back.

 

As shown below, press the Alt key while dragging a single dimension (A) in an alignment set (B) to move only that dimension.

 

16.png

 

When inserting callouts for blocks with custom properties like Cost, Material, etc. sometimes the actual text may appear as 'Error: Not Connected'. This can be resolved by Alt+dragging the callout handle and dropping it anywhere on the block.

 

17.png

 

Alt + Middle Click also fits the view to the screen.

Alt + Middle Drag also invokes the Zoom Area command.

 

Commands on the Ribbon bar can be accessed using the keyboard by tapping the Alt key which displays the key shortcuts for each tab, pressing which the Tab is activated and further key strokes required to access the commands are displayed.


The following work flow demonstrates the Zoom Fit command issued by Alt V F

 

18.png

 

Solid Edge is smart enough to add a shortcut key even for custom added ribbon buttons, so you can still use the Alt key (Alt C R for revision cloud) as seen below:

 

19.png

 

Note that its Alt V F and Alt C R and not Alt+C+R since the keys are not pressed in combination with Alt but in succession.

 

You can change the leader line attachment point using snap points displayed on the feature control frame. Pressing Alt while dragging the point (C) displays the snap points so you can connect to them.

20.png

 

 

Alt + Z invokes the Zoom tool 22.png

Upon invoking the Zool tool:

 

• Left click to Zoom In

Right click to Zoom Out

Left Drag to Zoom Area

Right Drag for Dynamic Pan

 

Two more uses by Imi from the comments section:

 

Alt + F5 restores the previous view.

 

Alt + Dragging a view disrupts or breaks the alignment with its parent view.

 

21.png

 

Ultimately, press Alt + F4 to quit Solid Edge !

 

Count  = 37

 

The list will be updated as and when I come across new uses for the Alt key in Solid Edge or when newer versions of Solid Edge bring in more uses to the Alt key.

 

Do mention in comments below your favourite Alt key uses in Solid Edge preferably explaining Why ?

 

Comments
Legend

Where do I find that revision cloud macro?

 

Gears Phenom

Hi,

 

This is very useful.

 

Here are some what I often use:

  • Alt + F5 - Restores the previous view
  • Alt + drag a drawing view - Deletes view alignment between selected and "main" drawing views
  • Ctrl + Alt + drag handle of projection line - Connects handle to new position with current value

 

BR,

Imi

Gears Phenom

Hi Imi, great observations. I have included those in the post. Please check.

However I found little differences when I tried out those.

Alt + Dragging a view did not delete the alignment but only disrupts or breaks it.

To delete an alignment, there is a right-click menu item on the view.

 

Also, your third use:

"Ctrl + Alt + drag handle of projection line - Connects handle to new position with current value"

I assume this is for a dimension. Ctrl + Alt + drag handle of projection line and connecting to new position changed the current value to display the new distance.

 

23.png

Regards,

Tushar

Gears Phenom

Hi,

 

I think I was not crystal clear.

 

Yes, you are right Alt + drag breaks alignment what is almost equal to delete. Smiley Wink

 

Here is a short video:

 

BR,

Imi

Gears Phenom

Thanks for the video, the Ctrl+Alt+Drag is a wonderful feature.

Another point to note is the local and online help differ.

There appears to be more documentation online.

Honored Contributor

Has a clean Alt baed menu tree been created? I would love to see one. I have consitered creating one, but expect it to take about 4 hours to do it right.

Gears Phenom

12GAGE, Alt based menu tree existed in Solid Edge before the Ribbon (Fluent) system came in.

What is that you said you consider creating in 4 hours and how?

Valued Contributor

Alt+drag the dimension end points to relocate to a new point is great. IN soldworks you didn't had to press Alt, simple drag would do. I always wondered that there must be a way to tdo this in Solid Edge. And here you @Tushar come with this article. Thanks

Gears Phenom

@Shiv_Madan

Not necessary. Each software has its own way of doing the same thing.

AutoCAD has a Shift+Drag for adjusting dimensions using hot and cold grips.